Software Download - live software from
dev.ti.comp. The live software currently works on Chrome®, Firefox®, and Safari® browsers. Internet Explorer® is not
supported. Users can access the live version through the link a Texas
Instruments' representative provides.
Click on the application icon within the gallery
to launch the software. Click on the prompt to install the TI Cloud Agent Bridge
browser plug-in.
Offline Software - users can access the
latest version of the offline software by navigating to the live version as
noted previously. Look for the download icon and download both the application
and runtime for the operating system as shown in Figure 3-1.
To be able to use the GUI properly, a USB2ANY
needs to be connected to the computer by the USB cable and connected to the EVM
via the 10-pin cable. For more information about the USB2ANY, see the USB2ANY
Interface Adapter User's Guide.
Figure 3-1 Download Icon for
TMUX7614D-SPI-EVM GUI