SCEA064A June 2019 – March 2021 2N7001T , SN74AXC4T245 , SN74AXC4T774 , TXB0104
A common use case for UART interfaces is as a communication link between devices.
An example is the communication between the circuits of a wireless speaker. The 2N7001T provides a simple solution for voltage level shifting between the processor and MCU. Figure 4-2 shows how an UART interface could be used for enabling the communication between the processor and the Wi-Fi block.