SCES551F February 2004 – March 2024 SN74AVC16T245
PRODUCTION DATA
Calculate the enable times for the SN74AVC16T45 using the following formulas:
In a bidirectional application, these enable times provide the maximum delay from the time the DIR bit is switched until an output is expected. For example, if the SN74AVC16T245 initially is transmitting from A to B, then the DIR bit is switched; the B port of the device must be disabled before presenting it with an input. After the B port has been disabled, an input signal applied to it appears on the corresponding A port after the specified propagation delay.