SCES642L December 2007 – November 2024 TXS0108E
PRODUCTION DATA
During operation, ensure that VCCA ≤ VCCB at all times. The sequencing of each power supply will not damage the device during the power up operation, so either power supply can be ramped up first. The output-enable (OE) input circuit is designed so that it is supplied by VCCA and when the (OE) input is low, all outputs are placed in the high-impedance state. To put the outputs in the high-impedance state during power up or power down, tie the OE input pin to GND through a pull-down resistor, and do not enable the OE input until VCCA and VCCB are fully ramped and stable. The current-sourcing capability of the driver determines the minimum value of the pull-down resistor to ground.