SCEU022A September 2020 – September 2022
Overall, this board is designed with ease-of-use and flexibility in mind. There is no one way to use this EVM to evaluate the multitude of devices it can support. Some users may find using the headers easy for them to interface with test equipment or connect to an external board, others will see benefit in using through-hole passive components to simulate expected loads for their system.
Some of the packages have thermal pads which were taken into account with this board design. These thermal pads were either grounded or left floating (depending on clearance constraints) which is the appropriate method for the devices being supported.