This section covers using InterConnect
Studio to permanently program a TPLD1201. Permanently programmed devices retain the
configuration the devices are programmed with after power is reset.
Permanently programmed devices must
not be permanently programmed again to avoid damaging the device.
- Open the desired configuration to
be permanently programmed in the TPLD1201 in InterConnect Studio.
- Open the Configure Settings by
selecting the three dots icon beside the CONFIGURE TPLD1201 button.
- Select Permanently Configure
Device. If using a TPLD-PROGRAM to power the EVM, then leave the Power
Source as Programmer. Select OK.
- Select the serial port connected
to the TPLD-PROGRAM, then select OK again.
- Some LEDs on the
TPLD1201-RWB-EVM can flash during the programming sequence, which is
normal.
- If the configuration
fails, then check the connections between the EVM and the computer, make
sure SW3 is ON, check the connection between the TPLD device and the
socket contacts, and retry.
- Remove power from the EVM before
removing the permanently programmed TPLD1201.