SFFS022 December 2022 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
Clock setup for the TMS320F2838xD/S MCU device family includes selecting the appropriate clock source, configuring the PLL multiplier, waiting for the lock status and switching the clock to the PLL output once the internal lock status is set. The time required for the PLL lock sequence can be profiled using on-chip timer to detect faults in the PLL wrapper logic. Once the PLL is locked, the frequency of the output clock can be checked by using the following: