SFFS022 December 2022 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The internal watchdog has two modes of operation: normal watchdog (WD) and windowed watchdog (WWD). The system integrator can select to use one mode or the other but not both at the same time. For details of programming the internal watchdogs, see the device-specific technical reference manual. The WD is a traditional single threshold watchdog. The user programs a timeout value to the watchdog and must provide a predetermined WDKEY to the watchdog before the timeout counter expires. Expiration of the timeout counter or an incorrect WDKEY triggers an error response. The WD can issue either a warm system reset or a CPU maskable interrupt upon detection of a failure. The WD is enabled after reset.
The use of the time window allows detection of additional clocking failure modes as compared to the WD implementation. User programs an upper bound and lower bound to create a time window during which the software must provide a predetermined WDKEY to the watchdog. Failure to receive the correct response within the time window or an incorrect WDKEY triggers an error response. The WWD can issue either a warm system reset or a CPU maskable interrupt upon detection of a failure. Normal WD operation is enabled by default after reset. For details of programming the internal watchdogs, see the device-specific technical reference manual.
In order to avoid common cause failure of clock input to both Internal Watchdog(WD) and CPU, it is recommended to select either INTOSC2 or X1/X2 as clock source to main PLL.