SFFS022 December 2022 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The VCU CRC diagnostic is based on a 32-bit polynomial. For a given test, only one code is valid out of 232 possibilities. Therefore, if there is a fault in the VCU CRC logic or associated data path, it is extremely unlikely that the correct passing code will be generated via the fault.