SFFS022 December 2022 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
Each CPU subsystem has a pair of diverse processing units (C28 and CLA) with different architecture and instruction set. This enables one processing unit to be used for handling the time critical portion code (control CPU) and other processing unit (supervisor CPU) to execute non critical portion of the code, perform diagnostic functions and supervise execution of the control CPU as indicated in Figure 3-6.
In case of identification of fault during diagnostic functions of the supervisor CPU, it can cause the MCU to move to a safe state. This concept, “reciprocal comparison by software in separate processing units” acts as a 1oo1D structure providing high diagnostic coverage for the processing units as per ISO26262-5, Table D.4. The comparison need to be performed several times during a FTTI. Reciprocal comparison is a software diagnostic feature and hence care should be taken to avoid common mode failures. The final attained coverage will depend on quality of comparison (determined by extend and frequency of cross checking). The proposed cross checking mechanism allows for hardware and software diversity since different processors with different instruction set and compiler is used for enabling this. The diversity can be further increased by having separate algorithms being executed in both the cores. In case, failure is identified during reciprocal comparison, NMI can be triggered by software and this in turn will assert ERRORSTS.