SFFS022 December 2022 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The General-Purpose Input/Output (GPIO) module provides software configurable mapping of internal module I/O functionality to device pins. These pins can be individually selected to operate as digital I/O (also called GPIO mode), or connected to one of several peripheral I/O signals.
The following tests can be applied as diagnostics for this module (to provide diagnostic coverage on a specific function):