SFFS022 December 2022 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
When this module transmits information onto its Bus, it can also monitor the Bus to ensure that the transmitted information is appearing as expected on the Bus. If the expected values are not read back from the Bus, the hardware can flag the error and signal an interrupt to the CPU. This feature must be enabled and configured in software.