SFFS034A July 2021 – July 2021 TPS1H000-Q1
This section provides a Failure Mode Analysis (FMA) for the pins of the TPS1H000-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality |
B | No device damage, but loss of functionality |
C | No device damage, but performance degradation |
D | No device damage, no impact to functionality or performance |
Figure 4-1 shows the TPS1H000-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TPS1H000-Q1 data sheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
IN | 1 | Normal operation with output off (FET turned off). | B |
DIAG_EN | 2 | Normal operation with diagnostics function disabled. | B |
FAULT | 3 | Open drain fault diagnostics cannot be reported. | B |
CL | 4 | Current limit defaults to internal limit. | C |
DELAY | 5 | Normal operation with device in holding mode as defined in the data sheet. | B |
GND | 6 | Resistor/diode network will be bypassed if present. | B |
OUT | 7 | Short to GND protection kicks in to protect the device. | B |
VS | 8 | Device will have no input supply and will not function. | B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
IN | 1 | Output will be shut off because the pin is pulled down internally. | B |
DIAG_EN | 2 | Diagnostics will be disabled as the pin is pulled down internally. | B |
FAULT | 3 | Open drain fault diagnostics cannot be reported. | B |
CL | 4 | Device will not be able to provide output current. | B |
DELAY | 5 | Normal operation with device in auto-retry mode because the pin is pulled up internally. | B |
GND | 6 | Resistor/diode network will be bypassed if present. | B |
OUT | 7 | Loss of ground detection engages and device shuts off. | B |
VS | 8 | Device will have no input supply and will not function. | B |
Pin Name | Pin No. | Shorted to | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|---|
IN | 1 | 2 (DIAG_EN) | IN will affect DIAG_EN and vice versa. Diagnostics and the channel will be enabled if pin voltage > VIH; diagnostics and channel will be disabled if pin voltage < VIL. | B |
DIAG_EN | 2 | 3 (FAULT) | Undefined device behavior depends on pin voltage. Diagnostics will be enabled if pin voltage > VIH; diagnostics will be disabled if pin voltage < VIL. Open drain fault reporting could not be correct. | B |
FAULT | 3 | 4 (CL) | Open drain fault reporting could not be correct. Current limit would not be anticipated value. | B |
DELAY | 5 | 6 (GND) | Device would be in the holding mode as defined in the data sheet. | B |
GND | 6 | 7 (OUT) | Short to ground protection would kick in. Device would be protected. | B |
OUT | 7 | 8 (VS) | Short to battery detection would be triggered if configured. Device cannot turn off output. | B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
IN | 1 | Normal operation with output turned on. | B |
DIAG_EN | 2 | Normal operation with diagnostics turned on. | B |
FAULT | 3 | Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell. | A |
CL | 4 | Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell. | A |
DELAY | 5 | Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell. | A |
GND | 6 | Supply power will be bypassed and device will not turn on. | B |
OUT | 7 | Output will be pulled to supply voltage. Short-to-battery detection will be triggered if configured. | B |
VS | 8 | Device functions as intended. | D |