SFFS061 February   2021 TLV759P

 

  1.   Trademarks
  2. 1Overview
  3. 2Functional Safety Failure In Time (FIT) Rates
  4. 3Failure Mode Distribution (FMD)
  5. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a Failure Mode Analysis (FMA) for the pins of the TLV759P. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to Ground (see Table 4-3)
  • Pin open-circuited (see Table 4-4)
  • Pin short-circuited to an adjacent pin (seeTable 4-5)
  • Pin short-circuited to supply (see Table 4-6)

Table 4-3 through Table 4-6 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
Class Failure Effects
A Potential device damage that affects functionality
B No device damage, but loss of functionality
C No device damage, but performance degradation
D No device damage, no impact to functionality or performance

Figure 4-1 shows the TLV759P pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TLV759P data sheet.

GUID-F2EE0D40-562D-4B17-A66C-926C6528C930-low.svg Figure 4-1 Pin Diagram for the TLV759P DRV Package [6 Pin Adjustable WSON]
Table 4-2 Pin Functions
Pin I/O DESCRIPTION
Name No.
OUT 1 OUTPUT Regulated Output
FB 2 - Input to the Control Loop Error Amplifier
GND 3 - Ground
EN 4 INPUT Drive Greater Than VEN(HIGH) to Turn On the Regulator. Drive Less Than VEN(LOW) to Put Regulator in Shutdown Mode
DNC 5 - Do Not Connect
IN 6 INPUT Inpur Supply
Thermal Pad Pad - Connect the thermal pad Ground for Improved Thermal Performance
Table 4-3 Pin FMA for Device Pins Short-Circuited to Ground
Pin Description of Potential Failure Effect(s) Failure Effect Class
Name No.
OUT 1 Output voltage will be near/at ground - Device will enter current limit. It may cycle in and out of thermal shutdown depending on power dissipation B
FB 2 Device will stop regulating. VOUT becomes equal to VIN minus dropout because the pass FET is driven on as hard as possible B
GND 3 - D
EN 4 Device will turn off B
DNC 5 - D
IN 6 No Output Voltage. Input Supply can be 0V B
Table 4-4 Pin FMA for Device Pins Open-Circuited
Pin Description of Potential Failure Effect(s) Failure Effect Class
Name No.
OUT 1 Output voltage is disconnected from load B
FB 2 Error amplifier input is left floating, output voltage will not equal to set voltage and will drift up to VIN minus a dropout voltage B
GND 3 Device may disable B
EN 4 Device may disable B
DNC 5 - D
IN 6 No output voltage B
Table 4-5 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Shorted To Pin No. Description of Potential Failure Effect(s) Failure Effect Class
Name No.
OUT 1 FB 2 VOUT will be set to VFB = 0.55 Vdc B
FB 2 GND 3 Device will stop regulating. VOUT becomes equal to VIN minus dropout because the pass FET is driven on as hard as possible B
GND 3 EN 4 Output is forced OFF, VOUT is 0.0V B
EN 4 DNC 5 - D
DNC 5 IN 6 - D
IN 6 OUT 1 Device will stop regulating. VOUT becomes equal to VIN B
Table 4-6 Pin FMA for Device Pins Short-Circuited to supply
Pin Description of Potential Failure Effect(s) Failure Effect Class
Name No.
OUT 1 Device will stop regulating. VOUT becomes equal to VIN B
FB 2 FB pin will be damaged if VIN is higher than 2V A
GND 3 Input supply will be driven to GND. No Output Voltage B
EN 4 Output is enabled regardless of external control logic on the enable pin B
DNC 5 - D
IN 6 No Effect D