SFFS063 June   2021 TCAN1046-Q1 , TCAN1046V-Q1

 

  1.   1
  2.   2
  3.   3
  4.   4
  5.   5

Pin Failure Mode Analysis (Pin FMA)

This section provides a Failure Mode Analysis (FMA) for the pins of the TCAN1046-Q1 and TCAN1046V-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 4-2 through Table 4-8 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality
BNo device damage, but loss of functionality
CNo device damage, but performance degradation
DNo device damage, no impact to functionality or performance

Figure 4-1 shows the TCAN1046-Q1 pin diagram , and Figure 4-2 shows the TCAN1046V-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TCAN1046-Q1/TCAN1046V-Q1 data sheet.

GUID-20210223-CA0I-MNSC-2RLG-KW9MJ1RCBNRM-low.jpg Figure 4-1 TCAN1046-Q1 Pin Diagram
GUID-20210223-CA0I-ZHZH-SBQL-PTCFRQHDF52P-low.jpg Figure 4-2 TCAN1046V-Q1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • VCC = 4.5 to 5.5V
  • VIO (if applicable) = 1.7 to 5.5V
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. (TCAN1046-Q1) Pin No. (TCAN1046V-Q1) Description of Potential Failure Effect(s) Failure Effect Class
TXD1 1 1 CAN1 will enter dominant time out mode. Unable to transmit data to the CAN1 bus. B
GND1 2 2 None D
VCC1 3 - CAN1 unpowered, high ICC current. B
VCC - 3 Device unpowered, high ICC current. B
RXD1 4 4 Internal damage possible, MCU may not be able to receive data from the RXD pin. Unable to receive data from CAN1 bus. A
TXD2 5 6 CAN2 will enter dominant time out mode. Unable to transmit data to the CAN2 bus. B
GND2 6 5 None D
VCC2 7 - CAN2 unpowered, high ICC current. B
RXD2 8 7 Internal damage possible, MCU may not be able to receive data from the RXD pin. Unable to receive data from CAN2 bus. A
CANL2 9 9 VO(REC) spec violated. Degraded EMC performance on CAN2 bus. C
CANH2 10 10 Device cannot drive dominant to CAN2 bus, no communication possible. B
STB2 11 8 STB2 stuck low, CAN2 bus unable to enter low-power mode. B
VIO - 11 Device will be in protected mode. Transceiver passive on both CAN1 and CAN2 bus. B
CANL1 12 12 VO(REC) spec violated. Degraded EMC performance on CAN1 bus. C
CANH1 13 13 Device cannot drive dominant to CAN1 bus, no communication possible. B
STB1 14 14 STB1 stuck low, CAN1 bus unable to enter low-power mode. B
Thermal Pad - - None D
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. (TCAN1046-Q1) Pin No. (TCAN1046V-Q1) Description of Potential Failure Effect(s) Failure Effect Class
TXD1 1 1 TXD1 pin defaults high, CAN1 bus state always recessive and unable to transmit data to CAN1 bus. B
GND1 2 2 CAN1 unpowered. B
VCC1 3 - CAN1 unpowered. B
VCC - 3 Device unpowered. B
RXD1 4 4 No RXD1 output, unable to receive data from CAN1 bus. B
TXD2 5 6 TXD2 pin defaults high, CAN2 bus state always recessive and unable to transmit data to CAN2 bus. B
GND2 6 5 CAN2 unpowered. B
VCC2 7 - CAN2 unpowered. B
RXD2 8 7 No RXD2 output, unable to receive data from CAN2 bus. B
CANL2 9 9 Device cannot drive dominant on CAN2 bus, unable to communicate. B
CANH2 10 10 Device cannot drive dominant on CAN2 bus, unable to communicate. B
STB2 11 8 STB2 pin defaults high, CAN2 portion stuck in low-power mode. B
VIO - 11 Device will be in protected mode, Transceiver passive on both CAN1 and CAN2 bus. B
CANL1 12 12 Device cannot drive dominant on CAN1 bus, unable to communicate. B
CANH1 13 13 Device cannot drive dominant on CAN1 bus, unable to communicate. B
STB1 14 14 STB1 pin defaults high, CAN1 portion stuck in low-power mode. B
Thermal Pad - - None D
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin TCAN1046-Q1
Pin NamePin No.Shorted toDescription of Potential Failure Effect(s)Failure Effect Class
TXD11GND1CAN1 bus will enter dominant time out mode. Unable to transmit data to CAN1 bus.B
GND12VCC1CAN1 unpowered, high ICC current.B
VCC13RXD1RXD1 output stuck high, unable to receive data from CAN1 bus.B
RXD1 4 TXD2 RXD1 output reflects the input to TXD2, a separate CAN transceiver. Information from CAN1 will not be received correctly. B
TXD2 5 GND2 CAN2 bus will enter dominant time out mode. Unable to transmit data to CAN2 bus. B
GND2 6 VCC2 CAN2 unpowered, high ICC current. B
RXD2 8 CANL2 Messages on RXD2 will be corrupted by CANL2. Reception of data from CAN2 bus will not be possible. IOS current may be reached. B
CANL2 9 CANH2 CAN2 bus stuck recessive, no communication possible. IOS current may be reached. B
CANH2 10 STB2 CAN2 driver and receiver turn off when a dominant is driven on CAN2 bus. May not enter normal mode. B
STB2 11 CANL1 CAN2 driver and receiver may turn off when the CAN1 bus is recessive. May not enter normal mode. B
CANL1 12 CANH1 CAN1 bus stuck recessive, no communication possible IOS current may be reached. B
CANH1 13 STB1 CAN1 driver and receiver turn off when a dominant is driven on CAN1 bus. May not enter normal mode. B
Note: The VSON package includes a thermal pad. All device pins are adjacent to the thermal pad. The device behavior when pins are shorted to the thermal pad depends on which net is connected to the thermal pad.
Table 4-5 Pin FMA for Device Pins Short-Circuited to Adjacent Pin TCAN1046V-Q1
Pin Name Pin No. Shorted to Description of Potential Failure Effect(s) Failure Effect Class
TXD1 1 GND1 CAN1 bus will enter dominant time out mode. Unable to transmit data to CAN1 bus. B
GND1 2 VCC Device unpowered, high ICC current. B
VCC 3 RXD1 RXD1 output stuck high, unable to receive data from CAN1 bus. B
RXD1 4 GND2 CAN1 receiver output stuck dominant. Unable to receive data from CAN1 bus. B
GND2 5 TXD2 CAN2 bus will enter dominant time out mode. Unable to transmit data to CAN2 bus. B
TXD2 6 RXD2 RXD2 output reflects the input to TXD2, and while this is the same transceiver, due to loop delay, the communication will be corrupted. Information from CAN2 bus will not be received correctly. B
STB2 8 CANL2 CAN2 driver and receiver may turn off when the CAN2 bus is recessive. May not enter normal mode. B
CANL2 9 CANH2 CAN2 bus stuck recessive, no communication possible. IOS current may be reached. B
CANH2 10 VIO CAN2 bus stuck dominant, no communication possible. B
VIO 11 CANL1 CAN1 bus stuck recessive, no communication possible. IOS current may be reached on CANL1. B
CANL1 12 CANH1 CAN1 bus stuck recessive, no communication possible IOS current may be reached. B
CANH1 13 STB1 CAN1 driver and receiver turn off when a dominant is driven. May not enter normal mode. B
Table 4-6 Pin FMA for Device Pins Short-Circuited to VCC
Pin Name Pin No. (TCAN1046-Q1) Pin No. (TCAN1046V-Q1) Description of Potential Failure Effect(s) Failure Effect Class
TXD1 1 1 TXD1 pin stuck high, unable to transmit data to CAN1 bus. B
GND1 2 2 CAN1 transceiver unpowered, high ICC current. B
VCC1 3 - None D
VCC - 3 None D
RXD1 4 4 RXD1 pin stuck high, unable to receive data from CAN1 bus. B
TXD2 5 6 TXD2 pin stuck high, unable to transmit data to CAN2 bus. B
GND2 6 5 CAN2 transceiver unpowered, high ICC current. B
VCC2 7 - None D
RXD2 8 7 RXD2 pin stuck high, unable to receive data for CAN2 bus. B
CANL2 9 9 CAN2 bus always recessive, no communication possible. IOS current may be reached. B
CANH2 10 10 VO(REC) spec violated, degraded EMC performance on CAN2 bus. C
STB2 11 8 STB2 stuck high, CAN2 transceiver always in standby mode. B
VIO - 11 IO pins will operate as 5V input/output. Microcontroller may be damaged if VCC > VIO. C
CANL1 12 12 CAN1 bus always recessive, no communication possible. IOS current may be reached. B
CANH1 13 13 VO(REC) spec violated, degraded EMC performance on CAN1 bus. C
STB1 14 14 STB1 stuck high, CAN1 transceiver always in standby mode.
Table 4-7 PIN FMA for Device Pins Short-Circuited to VIO
Pin Name Pin No. (TCAN1046V-Q1) Description of Potential Failure Effect(s) Failure Effect Class
TXD1 1 TXD1 stuck high, unable to transmit data to CAN1 bus. B
GND1 2 CAN1 unpowered, high IIO current. B
VCC 3 IO pins will operate as 5V input/output. Microcontroller may be damaged if VCC > VIO. C
RXD1 4 RXD1 pin stuck high, unable to receive data from CAN1 bus. B
GND2 5 CAN2 unpowered, high IIO current. B
TXD2 6 TXD2 stuck high, unable to transmit data to CAN2 bus. B
RXD2 7 RXD2 pin stuck high, unable to receive data from CAN2 bus. B
STB2 8 STB2 stuck high, CAN2 transceiver always in standby mode. B
CANL2 9 CAN2 bus always recessive, no communication possible. IOS current may be reached if VIO ≥ 3.3V. B
CANH2 10 VO(REC) spec violated if VIO ≥ 3.3V, degraded EMC performance on CAN2 bus. C
VIO 11 None D
CANL1 12 CAN1 bus always recessive, no communication possible. IOS current may be reached if VIO ≥ 3.3V. B
CANH1 13 VO(REC) spec violated if VIO ≥ 3.3V, degraded EMC performance on CAN1 bus. C
STB1 14 STB1 stuck high, CAN1 transceiver always in standby mode. B
Table 4-8 Pin FMA for Device Pins Short-Circuited to VBAT
Pin Name Pin No. (TCAN1046-Q1) Pin No. (TCAN1046V-Q1) Description of Potential Failure Effect(s) Failure Effect Class
TXD1 1 1 Absolute maximum violation, transceiver may be damaged. Unable to transmit data to CAN1 bus. A
GND1 2 2 Device unpowered, high IBAT current. B
VCC1 3 - Absolute maximum violation, transceiver may be damaged. CAN1 bus may be unable to communicate. A
VCC - 3 Absolute maximum violation, transceiver may be damaged. CAN bus may be unable to communicate. A
RXD1 4 4 Absolute maximum violation, transceiver may be damaged. Unable to receive data from CAN1 bus. A
TXD2 5 6 Absolute maximum violation, transceiver may be damaged. Unable to transmit data to CAN2 bus. A
GND2 6 5 Device unpowered, high IBAT current. B
VCC2 7 - Absolute maximum violation, transceiver may be damaged. CAN2 bus may be unable to communicate. A
RXD2 8 7 Absolute maximum violation, transceiver may be damaged. Unable to receive data from CAN2 bus. B
CANL2 9 9 CAN2 bus always recessive, no communication possible. IOS current may be reached. B
CANH2 10 10 VO(REC) spec violated, degraded EMC performance on CAN2 bus. C
STB2 11 8 Absolute maximum violation, transceiver may be damaged. CAN2 transceiver stuck in standby mode. A
VIO - 11 Absolute maximum violation, transceiver may be damaged. A
CANL1 12 12 CAN1 bus always recessive, no communication possible. IOS current may be reached. B
CANH1 13 13 VO(REC) spec violated, degraded EMC performance on CAN1 bus. B
STB1 14 14 Absolute maximum violation, transceiver may be damaged. CAN1 transceiver stuck in standby mode. A