SFFS138 December 2021 TCAN1164-Q1
The device has short circuit current limit (IL_VCCOUT), which limits the maximum amount of current that can be sourced by the LDO. Depending on bus state/fault and ambient temperature, that prolonged time at IL_VCCOUT could eventually trigger a thermal shutdown (TSD) event if the additional current load heats the die up enough.