SFFS141 December 2021 TCAN1167-Q1
The TCAN1167-Q1 has 6 digital I/O pins, four of which are used to implement the SPI communications and the other two are utilized for the TXD and RXD signals for the CAN. These digital I/Os operate on the VCCOUT pin. Four of these input pins have integrated pull-up resistors that weakly bias them.
The following sections provide the functional safety mechanisms that cover the digital inputs and outputs: