SFFS203 September 2022 TLV1812 , TLV1822
This section provides a Failure Mode Analysis (FMA) for the pins of the TLV1812 and TLV1822. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Pin short-circuited to supply pin (see Table 4-5)
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality |
B | No device damage, but loss of functionality |
C | No device damage, but performance degradation |
D | No device damage, no impact to functionality or performance |
Figure 4-1 shows the TLV1812 and TLV1822 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TLV1812 and TLV1822 data sheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
OUT1 |
1 |
Thermal stress due to high power dissipation (Push-Pull) No change if same node as V- (Open-Drain) |
A B |
IN1- |
2 |
Output goes high, if other input is positive |
B |
IN1+ |
3 |
Output goes low, if other input is positive |
B |
V- |
4 |
No change if same node as V- |
D |
IN2+ |
5 |
Output goes low, if other input is positive |
B |
IN2- |
6 |
Output goes high, if other input is positive |
B |
OUT2 |
7 |
Thermal stress due to high power dissipation (Push-Pull) No change if same node as V- (Open-Drain) |
A B |
V+ |
8 |
Main supply shorted out (no power to device) |
B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
OUT1 |
1 |
Output can't drive application load |
B |
IN1- |
2 |
Output may be low or high |
B |
IN1+ |
3 |
Output may be low or high |
B |
V- |
4 |
Highest voltage pin will drive V- pin internally (via diode) |
B |
IN2+ |
5 |
Output may be low or high |
B |
IN2- |
6 |
Output may be low or high |
B |
OUT2 |
7 |
Output can't drive application load |
B |
V+ |
8 |
Main supply open (no power to device) |
B |
Pin Name | Pin No. | Shorted to | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|---|
OUT1 to IN1- |
1 |
2 |
Output may be low or high |
B |
IN1- to IN1+ |
2 |
3 |
Output may be low or high |
B |
IN1+ to V- |
3 |
4 |
Output goes low, if other input is positive |
B |
V- to IN2+ |
4 |
5 |
Output goes low, if other input is positive |
B |
IN2+ to IN2- |
5 |
6 |
Output may be low or high |
B |
In2- to OUT2 |
6 |
7 |
Output may be low or high |
B |
OUT2 to V+ |
7 |
8 |
Thermal stress due to high power dissipation |
A |
V+ to OUT1 |
8 |
1 |
Thermal stress due to high power dissipation |
A |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
OUT1 |
1 |
Thermal stress due to high power dissipation |
A |
IN1- |
2 |
Output goes low, if other input is less positive |
B |
IN1+ |
3 |
Output goes high, if other input is less positive |
B |
V- |
4 |
Main supply shorted out (no power to device) |
B |
IN2+ |
5 |
Output goes high, if other input is less positive |
B |
IN2- |
6 |
Output goes low, if other input is less positive |
B |
OUT2 |
7 |
Thermal stress due to high power dissipation |
A |
V+ |
8 |
No change if same node as V+ |
D |