SFFS240A August 2022 – October 2022 TPS55288-Q1 , TPS552882-Q1
This section provides a Failure Mode Analysis (FMA) for the pins of the TPS55288-Q1 and TPS552882-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality |
B | No device damage, but loss of functionality |
C | No device damage, but performance degradation |
D | No device damage, no impact to functionality or performance |
Figure 4-1 and Figure 4-2 show the TPS55288-Q1 and TPS552882-Q1 pin diagrams. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TPS55288-Q1 36-V, 16-A Buck-Boost Converter with I2C Interface and TPS552882-Q1 36-V, 16-A Buck-Boost Converter data sheets.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
Device used within the Recommended Operating Conditions and the Absolute Maximum Ratings found in the TPS55288-Q1 36-V, 16-A Buck-Boost Converter with I2C Interface and TPS552882-Q1 36-V, 16-A Buck-Boost Converter data sheets.
Configuration as shown in the Application and Implementation found in the TPS55288-Q1 36-V, 16-A Buck-Boost Converter with I2C Interface and TPS552882-Q1 36-V, 16-A Buck-Boost Converter data sheets.
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
DR1L | 1 | Possible device damage | A |
DR1H | 2 | No output voltage | B |
VIN | 3 | The device does not operate. Power supply is short. | B |
EN/UVLO | 4 | Loss of ENABLE functionality. The device remains in shutdown mode. | B |
SCL | 5 | For the TPS55288-Q1, there is no output voltage. | B |
PG | For the TPS552882-Q1, this is the correct output voltage. Loss of power-good indication functionality | C | |
SDA | 6 | For the TPS55288-Q1, there is no output voltage. | B |
CC | For TPS552882-Q1, this is the correct output voltage. Loss of constant current output indication functionality | C | |
DITH/SYNC | 7 | Correct output voltage. Loss of DITH/SYNC functionality | C |
FSW | 8 | Possible device damage | A |
PGND | 9 | No effect | D |
AGND | 10 | The internal circuit can be disturbed. | C |
VOUT | 11 | The device remains in hiccup output short circuit protection mode. | B |
ISP | 12 | The device remains in hiccup output short circuit protection mode. | B |
ISN | 13 | No output voltage | B |
FB/INT | 14 | For the TPS55288-Q1, when internal feedback is used, this pin always indicates low even in the normal condition. When external feedback is used, OVP is triggered. | B |
FB | For the TPS552882-Q1, OVP is triggered. | B | |
MODE | 15 | For the TPS55288-Q1, the device always works in FPWM mode with I2C target address 74H, but no output voltage with I2C target address 75H. | B |
For the TPS552882-Q1, the device remains in FPWM mode and internal VCC source. Loss of PFM mode and external VCC source functionality. | C | ||
CDC | 16 | For the TPS55288-Q1, there is no effect when internal CDC compensation is used, but loss of the cable voltage drop compensation and the output voltage is overcompensated when external CDC compensation is used. | C |
For the TPS552882-Q1, there is loss of the cable voltage drop compensation functionality and the output voltage is overcompensated. | B | ||
ILIM | 17 | Potential damage to inductor and chip | A |
COMP | 18 | The output voltage is out of regulation. If in FPWM, the converter works in minimum tON. If in PFM, there is no switching. | B |
VCC | 19 | The device does not operate. VCC is short. | B |
BOOT2 | 20 | No output voltage | B |
SW2 | 21 | Possible device damage | A |
BOOT1 | 22 | No output voltage | B |
SW1 | 23 | Possible device damage | A |
PGND | 24 | No effect | D |
SW2 | 25 | Possible device damage | A |
VOUT | 26 | The device remains in hiccup output short circuit protection mode. | B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
DR1L | 1 | Correct output voltage. Efficiency is lower. | C |
DR1H | 2 | No output voltage | B |
VIN | 3 | The device does not work and there is no output voltage. | B |
EN/UVLO | 4 | No output voltage. Loss of ENABLE functionality | B |
SCL | 5 | For the TPS55288-Q1, there is no output voltage. | B |
PG | For the TPS552882-Q1, this is the correct output voltage. Loss of power-good indication functionality | C | |
SDA | 6 | For the TPS55288-Q1, there is no output voltage. | B |
CC | For the TPS552882-Q1, this is the correct output voltage. Loss of constant current output indication functionality | C | |
DITH/SYNC | 7 | Correct output voltage. Loss of DITH/SYNC functionality | C |
FSW | 8 | No output voltage | B |
PGND | 9 | Possible device damage | A |
AGND | 10 | Possible device damage | A |
VOUT | 11 | Possible device damage | A |
ISP | 12 | No output voltage | B |
ISN | 13 | The output voltage is out of regulation. | B |
FB/INT | 14 | For the TPS55288-Q1, there is a loss of the FAULT indicator function when internal feedback is used. OVP is triggered when external feedback is used. | B |
FB | For the TPS552882-Q1, OVP is triggered. | B | |
MODE | 15 | For the TPS55288-Q1, the device always works in PFM mode with I2C target address 75H and external VCC source. No output with I2C target address 74H. | B |
For the TPS552882-Q1, the device remains in PFM mode and external VCC source. Loss of FPWM mode and internal VCC source functionality | C | ||
CDC | 16 | Loss of CDC functionality and no cable voltage drop compensation | C |
ILIM | 17 | The output current capability decreases. | B |
COMP | 18 | Output voltage is out of regulation. | B |
VCC | 19 | Possible device damage | A |
BOOT2 | 20 | Efficiency is lower. | B |
SW2 | 21 | Possible device damage | A |
BOOT1 | 22 | Possible device damage | A |
SW1 | 23 | Possible device damage | A |
PGND | 24 | Possible device damage | A |
SW2 | 25 | Possible device damage | A |
VOUT | 26 | Possible device damage | A |
Pin Name | Pin No. | Shorted to | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|---|
DR1L | 1 | DR1H | No output voltage | B |
DR1H | 2 | VIN | Possible device damage | A |
VIN | 3 | EN/UVLO | The EN/UVLO pin is damaged if VIN is higher than 20 V. | A |
EN/UVLO | 4 | SCL | For the TPS55288-Q1, the SCL pin is damaged if EN/UVLO is higher than 6 V. | A |
PG | For the TPS552882-Q1, the PG pin is damaged if EN/UVLO is higher than 6 V. | A | ||
SCL | 5 | SDA | For the TPS55288-Q1, there is no output voltage. | B |
PG | CC | For the TPS552882-Q1, this is the correct output voltage. Loss of PG and CC functionality | C | |
SDA | 6 | DITH/SYNC | For the TPS55288-Q1, this is the correct output voltage. Loss of DITH/SYNC functionality | C |
CC | For the TPS552882-Q1, this is the correct output voltage. Loss of CC and DITH/SYNC functionality | C | ||
DITH/SYNC | 7 | FSW | Possible device damage | A |
FSW | 8 | PGND | Possible device damage | A |
PGND | 9 | AGND | The internal circuit can be disturbed. | C |
AGND | 10 | VOUT | The device remains in hiccup output short circuit protection mode and the internal circuit can be disturbed. | B |
VOUT | 11 | ISP | Output current limit accuracy is affected. | C |
ISP | 12 | ISN | Correct output voltage. Loss of output current limit functionality | C |
ISN | 13 | FB/INT | For the TPS55288-Q1, the FB/INT pin damaged if ISN is higher than 6 V. | A |
FB | For the TPS552882-Q1, output voltage equals 1.2 V. | B | ||
FB/INT | 14 | MODE | For the TPS55288-Q1, no output voltage when internal feedback is used. When external feedback is used, OVP is triggered. | B |
FB | For the TPS552882-Q1, OVP is triggered. | B | ||
MODE | 15 | CDC | Loss of CDC functionality and output voltage is out of regulation. | B |
CDC | 16 | ILIM | Incorrect current limit setting and CDC compensation | B |
ILIM | 17 | COMP | Output voltage is out of regulation. | B |
COMP | 18 | VCC | OVP is triggered. | B |
VCC | 19 | BOOT2 | The VCC pin is damaged if BOOT2 is higher than 6 V. | A |
BOOT2 | 20 | SW2 | Efficiency is lower because the boost HFET is always off. | C |
SW2 | 21 | BOOT1 | Possible device damage | A |
BOOT1 | 22 | SW1 | Output voltage is out of regulation. | B |
SW1 | 23 | DR1L | Possible device damage if SW1 is higher than 6 V | A |
PGND | 24 | SW2 | Potential device damage | A |
SW2 | 25 | VOUT | Possible device damage | A |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
DR1L | 1 | The DR1L pin is damaged if supply voltage is higher than 6 V. | A |
DR1H | 2 | Possible device damage | A |
VIN | 3 | No effect | D |
EN/UVLO | 4 | The EN/UVLO pin is damaged if supply voltage is higher than 20 V. | A |
SCL | 5 | For the TPS55288-Q1, the SCL pin is damaged if supply voltage is higher than 6 V. | A |
PG | For the TPS552882-Q1, the PG pin is damaged if supply voltage is higher than 6 V. | A | |
SDA | 6 | For the TPS55288-Q1, the SDA pin is damaged if supply voltage is higher than 6 V. | A |
CC | For the TPS552882-Q1, the CC pin is damaged if supply voltage is higher than 6 V. | A | |
DITH/SYNC | 7 | The DITH/SYNC pin is damaged if supply voltage is higher than 6 V. | A |
FSW | 8 | The FSW pin is damaged if supply voltage is higher than 6 V. | A |
PGND | 9 | The device does not operate. Power supply is short. | B |
AGND | 10 | The device does not operate. Power supply is short. | B |
VOUT | 11 | The VOUT pin is damaged if supply voltage is higher than 25 V. The output voltage is equal to the supply voltage. | A |
ISP | 12 | The ISP pin is damaged if supply voltage is higher than 25 V. The output voltage is equal to the supply voltage. | A |
ISN | 13 | The ISN pin damaged if supply voltage is higher than 25 V. The output voltage is equal to the supply voltage. | A |
FB/INT | 14 | For the TPS55288-Q1, the FB/INT pin is damaged if supply voltage is higher than 6 V. | A |
FB | For the TPS552882-Q1, the FB pin is damaged if supply voltage is higher than 6 V. | A | |
MODE | 15 | The MODE pin is damaged if supply voltage is higher than 6 V. | A |
CDC | 16 | The CDC pin is damaged if supply voltage is higher than 6 V. | A |
ILIM | 17 | The ILIM pin is damaged if supply voltage is higher than 6 V. | A |
COMP | 18 | The COMP pin is damaged if supply voltage is higher than 6 V. | A |
VCC | 19 | The VCC pin is damaged if supply voltage is higher than 6 V. | A |
BOOT2 | 20 | The BOOT2 pin is damaged if supply voltage is higher than 31 V. | A |
SW2 | 21 | The SW2 pin is damaged if supply voltage is higher than 25 V and internal power FETs are damaged. | A |
BOOT1 | 22 | Possible device damage | A |
SW1 | 23 | Damage to internal power FETs | A |
PGND | 24 | The device does not operate. Power supply is short. | B |
SW2 | 25 | The SW2 pin is damaged if supply voltage is higher than 25 V and internal power FETs are damaged. | A |
VOUT | 26 | The VOUT pin damaged if supply voltage is higher than 25 V. The output voltage is equal to the supply voltage. | A |