SFFS277 November 2023 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
The on-chip flash memory is supported by single error correction, double error detection (SECDED) error correcting code (ECC) diagnostic. In this SECDED scheme, an 8-bit code word is used to store the ECC of 64 bit data and corresponding address. The ECC decoding logic at the flash bank output checks the correctness of memory content. ECC evaluation is done on every data and program read. The data and program interconnects that connect the CPU and flash memory is not protected by ECC. Detected correctable errors can be corrected or not corrected, depending on whether correction functionality is enabled. Single bit address ECC errors are flagged as uncorrectable errors. Errors that cannot be corrected will generate an NMI and ERRORSTS pin is asserted. Count of the corrected errors (single bit data errors) is monitored by the flash wrapper and an interrupt is generated once the count exceeds the programmed threshold. The corrupted memory address of the last error location is also logged in flash wrapper.