SFFS277 November 2023 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
The standardized E-GAS monitoring concept [6] for engine management systems generated by the German VDA working group “E-Gas-Arbeitskreis” is an example of a well-trusted safety-architecture that may be used for applications other than engine management systems provided it fits the purpose of the new application in terms of diagnosis feasibility, environment constraints, time constraints, robustness, and so forth [7]. For more information, see Figure 4-3.
The MCU device family supports heterogeneous asymmetric architecture and their functional safety features lend themselves to an E-GAS concept implementation at system level as indicated in Figure 4-4. In the first level (Level 1), the functions required for the system mission are computed. Second level (Level 2) checks the correct formation in first level based on selected set of parameters. Third level (Level 3) implements an additional external monitoring element, for the correct carrying out of the mission in the first level and/or monitoring in the second level. The exact functional safety implementation and the modules used for realizing Level 1 and Level 2 and the external monitoring device for realizing Level 3 are left to the system designer.
Due to the inherent versatility of the device architecture, several software voting based functional safety configurations are possible. Some of the functional safety configurations possible with TMS320F28003x for improving diagnostic coverage are explained in Table 8-1. While implementing these configurations, system integrator needs to consider the potential common mode failures and address them in an appropriate manner. This may suitably be modified to adapt to TMS320F28003x requirements based on the availability of processing units. (As stated earlier, the device claims no hardware fault tolerance, (for example, no claims of HFT > 0), as defined in IEC 61508:2010).
The major safety features of TMS320F28003x are shown in Figure 4-5.