SFFS277 November 2023 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
PLL Lock functionality is implemented by comparing the difference (error) between the feedback clock and reference clock through Phase Frequency Detector (PFD). When PLL is in lock and generating the correct frequency, the difference is <100pS~300pS. Once there is any fault causing the PLL output frequency to drift, the difference will go outside of that range. In such a case, PLL Lock signal will go from 1 to 0 indicating PLL is out of lock. DCC can be used to detect that drift has occurred.