SFFS277 November 2023 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
The source code delivered with the CLA_STL must be validated with the reference MD5 information provided in SDF file for each STL. The SDF file is delivered as part of the CSP. A unique MD5 signature applies to each of the source files used to create the Self Test Libraries. Checking the MD5 signature is strongly recommended as a precautionary step to ensure that the source code is exactly the same as what was certified by TÜV SÜD.
In order to ensure that the required diagnostic coverage based metrics are achieved, the source must not be modified in anyway and is expected to be used as is. Violating this condition will result in a potential failure in the operation of the CLA_STL and it may not meet the required safety requirements.