SFFS282 September 2022 TLV1812-Q1 , TLV1822-Q1
This section provides a Failure Mode Analysis (FMA) for the pins of the TLV1812-Q1 and TLV1822-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Pin short-circuited to supply pin (see Table 4-5)
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality |
B | No device damage, but loss of functionality |
C | No device damage, but performance degradation |
D | No device damage, no impact to functionality or performance |
Figure 4-1 shows the TLV1812-Q1 and TLV1822-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TLV1812-Q1 and TLV1822-Q1 data sheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
OUT1 |
1 |
Thermal stress due to high power dissipation (Push-Pull) No change if same node as V- (Open-Drain) |
A B |
IN1- |
2 |
Output goes high, if other input is positive |
B |
IN1+ |
3 |
Output goes low, if other input is positive |
B |
V- |
4 |
No change if same node as V- |
D |
IN2+ |
5 |
Output goes low, if other input is positive |
B |
IN2- |
6 |
Output goes high, if other input is positive |
B |
OUT2 |
7 |
Thermal stress due to high power dissipation (Push-Pull) No change if same node as V- (Open-Drain) |
A B |
V+ |
8 |
Main supply shorted out (no power to device) |
B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
OUT1 |
1 |
Output can't drive application load |
B |
IN1- |
2 |
Output may be low or high |
B |
IN1+ |
3 |
Output may be low or high |
B |
V- |
4 |
Highest voltage pin will drive V- pin internally (via diode) |
B |
IN2+ |
5 |
Output may be low or high |
B |
IN2- |
6 |
Output may be low or high |
B |
OUT2 |
7 |
Output can't drive application load |
B |
V+ |
8 |
Main supply open (no power to device) |
B |
Pin Name | Pin No. | Shorted to | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|---|
OUT1 to IN1- |
1 |
2 |
Output may be low or high |
B |
IN1- to IN1+ |
2 |
3 |
Output may be low or high |
B |
IN1+ to V- |
3 |
4 |
Output goes low, if other input is positive |
B |
V- to IN2+ |
4 |
5 |
Output goes low, if other input is positive |
B |
IN2+ to IN2- |
5 |
6 |
Output may be low or high |
B |
In2- to OUT2 |
6 |
7 |
Output may be low or high |
B |
OUT2 to V+ |
7 |
8 |
Thermal stress due to high power dissipation |
A |
V+ to OUT1 |
8 |
1 |
Thermal stress due to high power dissipation |
A |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
OUT1 |
1 |
Thermal stress due to high power dissipation |
A |
IN1- |
2 |
Output goes low, if other input is less positive |
B |
IN1+ |
3 |
Output goes high, if other input is less positive |
B |
V- |
4 |
Main supply shorted out (no power to device) |
B |
IN2+ |
5 |
Output goes high, if other input is less positive |
B |
IN2- |
6 |
Output goes low, if other input is less positive |
B |
OUT2 |
7 |
Thermal stress due to high power dissipation |
A |
V+ |
8 |
No change if same node as V+ |
D |