SFFS302 October 2021 SN74LVC1G3157-Q1
Figure 4-1 and Figure 4-2 shows the SN74LVC1G3157-Q1 pin diagram for the DBV and DCK package. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the SN74LVC1G3157-Q1 data sheet.
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
B2 | 1 | Corruption of analog signal on B2 pin. If there is no limiting resistor in the switch path device damage is possible. | A |
GND | 2 | No effect, normal operation. | D |
B1 | 3 | Corruption of analog signal on B1 pin. If there is no limiting resistor in the switch path device damage is possible. | A |
A | 4 | Corruption of analog signal on A pin. If there is no limiting resistor in the switch path device damage is possible. | A |
VCC | 5 | Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible. | A |
S | 6 | S pin stuck to GND. Cannot control switch states. | B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
B2 | 1 | Corruption of analog signal on B2 pin. | B |
GND | 2 | Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible. | A |
B1 | 3 | Corruption of analog signal on B1 pin. | B |
A | 4 | Corruption of analog signal on A pin. | B |
VCC | 5 | Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible. | A |
S | 6 | Loss of control on Select pin. Switch in undefined state. | B |
Pin Name | Pin No. | Shorted to | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|---|
B2 | 1 | GND | Corruption of analog signal on B2 pin. If there is no limiting resistor in the switch path device damage is possible. | A |
GND | 2 | B1 | Corruption of analog signal on B1 pin. If there is no limiting resistor in the switch path device damage is possible. | A |
B1 | 3 | A | Not considered corner pin. | D |
A | 4 | VCC | Corruption of analog signal on A pin. If there is no limiting resistor in the switch path device damage is possible. | A |
VCC | 5 | S | Select pin stuck high. Cannot control switch states. | B |
S | 6 | B2 | Not considered corner pin. | D |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
B2 | 1 | Corruption of analog signal on B2. If there is no limiting resistor in the switch path device damage is possible. | A |
GND | 2 | Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible. | A |
B1 | 3 | Corruption of analog signal on B1. If there is no limiting resistor in the switch path device damage is possible. | A |
A | 4 | Corruption of analog signal on A. If there is no limiting resistor in the switch path device damage is possible. | A |
VCC | 5 | No effect, normal operation | D |
S | 6 | S pin stuck to VCC. Cannot control switch states. | B |