SFFS624A March 2024 – December 2024 MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
In this method, when the timer is idle, the polarity of the fault pin can be changed (FCTL.FSENEXTx) to the alternate value. This triggers a fault that can be checked by reading the status register. This method can be used to check if the fault detection circuit is working as expected.