SFFS624A March 2024 – December 2024 MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
In this method, the same signal is connected to two different comparators. The outputs from the two comparators are compared in the interrupt routine. By using two comparators to monitor the same signal, a fault in one of the comparators can be detected, even if one of the comparators is faulty, because the other comparator can still respond.