SFFS624A March 2024 – December 2024 MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
This test checks if the window comparator is working. As part of the ADC2 test, or a separate test, the ADC2 can be set so the threshold results in the ADC crossing the predefined thresholds. The test can check if the window comparator logic detects these conditions.