SFFS624A March 2024 – December 2024 MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
In the case where timing parameters of safety-critical inputs are measured, two or more spins can be connected to the same signal (redundancy), and the measured parameters (in different timer instances) can be compared to determine if the parameters are within the acceptable range. Input capture must be done on different timer instances. This covers faults in the clock divider as the measured timing parameters deviate from the expected values on the second instance.