SFFS659 December 2024 DRV5056-Q1
Figure 4-2 shows the DRV5056-Q1 pin diagram for the TO-92 package. For a detailed description of the device pins, see the Pin Configuration and Functions section in the DRV5056-Q1 data sheet.
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
VCC | 1 | Supply shorted to Ground. System will source high current as a result and may current limit. Thermal damage may result. B | B |
GND | 2 | Normal Mode of operation | D |
OUT | 3 | DRV5056-Q1 will not be damaged. Output will be pulled down by short to GND. | C |
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
VCC | 1 | DRV5056-Q1 will not be damaged. There will be no power supply current and therefore no functionality. | B |
GND | 2 | DRV5056-Q1 will not be damaged. There will be no power supply current and therefore no functionality. | B |
OUT | 3 | DRV5056-Q1 will not be damaged. Supply current will be normal, but the output is not driving any load. | C |
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
VCC | 1 | Normal mode of operation | D |
GND | 2 | Supply shorted to Ground. System will source high current as a result and may current limit. Thermal damage may result. | B |
OUT | 3 | DRV5056-Q1 will not be damaged. The output will sink about 14 mA (limited by overcurrent protection feature). The output signal will be pulled to VCC. Any MCU monitoring the output would observe VCC as an input which may result in over voltage. | B |