SFFS668 June 2024 LMR36503E-Q1
This section provides a failure mode analysis (FMA) for the pins of the LMR36503E-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality |
B | No device damage, but loss of functionality |
C | No device damage, but performance degradation |
D | No device damage, no impact to functionality or performance |
Figure 4-1 shows the LMR36503E-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the LMR36503E-Q1 data sheet.
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
RT or MODE | 1 | Switching frequency is 2.2MHz | D |
PGOOD | 2 | When not in use, can be left grounded (PGOOD is not a valid signal, VOUT normal) | D |
EN/UVLO | 3 | VOUT = 0V (Enable is off, functionality is halted) | D |
VIN | 4 | VOUT = 0V | B |
SW | 5 | Damage HSFET | A |
BOOT | 6 | VOUT = 0V, HS does not turn on | B |
VCC | 7 | VOUT = 0V | B |
VOUT/BIAS or FB | 8 | VOUT = 0V | B |
GND | 9 | VOUT normal | B |
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
RT or MODE | 1 |
For an RT part, frequency is not defined For a MODE/SYNC part, part can go back and forth between FPWM and PFM Part is up, part is functional | D |
PGOOD | 2 | When not in use, can be left open ( PGOOD is not a valid signal, VOUT normal) | D |
EN/UVLO | 3 | Pin cannot be left floating | B |
VIN | 4 | VOUT = 0V | B |
SW | 5 | VOUT = 0V | B |
BOOT | 6 | VOUT = 0V, HS does not turn on | B |
VCC | 7 | VCC output is unstable, can increase above 5.5V | A |
VOUT/BIAS or FB | 8 | VOUT = 0V. Do not float this pin | C |
GND | 9 | VOUT can be abnormal, as reference voltage is not fixed | C |
Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|---|
RT or MODE | 1 | PGOOD |
If PGOOD is high and < 5.5V, Fsw = 1MHz If PGOOD is low, Fsw = 2.2MHz PGOOD absolute maximum is 20V, RT ESD damage can occur when PG goes to 20V | A |
PGOOD | 2 | EN/UVLO | If EN/UVLO > 20V, devices connected to PGOOD pin can be damaged | A |
EN/UVLO | 3 | VIN | VOUT normal (Enable is on, all other blocks work) | D |
VIN | 4 | SW | Damage LSFET | A |
SW | 5 | BOOT | VOUT = 0V, HS does not turn on, no Cboot | B |
BOOT | 6 | VCC | Damage occurs, break VCC Pin | A |
VCC | 7 | VOUT/BIAS or FB | Does not work, but no damage occurs | B |
VOUT/BIAS or FB | 8 | GND | VOUT = 0V | B |
GND | 9 | RT or MODE | VOUT normal if RT/MODE/SYNC pin is low, otherwise not functional | B |
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
RT or MODE | 1 |
If Vin > 5.5V, damage occurs. If Vin < 5.5V, switching frequency is 1MHz | A |
PGOOD | 2 | If VIN > 20V, damage to PGOOD occurs | A |
EN/UVLO | 3 | VOUT normal (Enable is on, all other blocks work) | D |
VIN | 4 | VOUT normal | D |
SW | 5 | Damage LSFET | A |
BOOT | 6 | Damage occurs, BOOT ESD clamp is damaged | A |
VCC | 7 | If Vin > 5.5V, damage occurs | A |
VOUT/BIAS or FB | 8 | If VIN > 20V, damage occurs | A |
GND | 9 | VOUT = 0V | B |