SFFS700 May 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
LIN module supports detection of parity error on ID field. If parity is enabled, an ID parity error (PE) is detected if any of the two parity bits (even/odd) of the sent ID byte are not equal to the calculated parity on the receiver node. The two parity bits (even/odd) are generated using the mixed parity algorithm. If an ID parity error is detected, the ID parity error is flagged and the received ID is not valid