SFFS700 May 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The HWBIST diagnostic is based on a 512-bit signature capture. For a given test, only one code is valid out of 2512 possibilities. Therefore, if there is a fault in the HWBIST logic, it is extremely unlikely that the correct passing code will be generated via the fault. The cyclical check applied by the HWBIST module provides an inherent level of self-checking (auto-coverage), which can be considered for application in latent fault diagnostics.