The LEDs in the system should be
properly controlled to prevent a bright image. In cases where proper control is not
possible, the illumination should be turned off.
The DLP4620S-Q1 chipset includes several features to
monitoring the illumination control and turn off the LEDs in case of a fault.
Figure 6-6 and Figure 6-7 show the illumination control and LED driver architecture. Figure 6-8 shows the origin and destination of software, data, and settings.
As seen in Figure 6-6, Figure 6-7, and Figure 6-8:
- At start-up, the Boot ROM
commands External Flash to load the Main Application Software and
calibration data into the internal RAM (IRAM) of the DLPC231S-Q1. The ARM Core in the DLPC231S-Q1 executes the main application loaded in to the
IRAM.
- The host MCU sends dimming
commands periodically to the DLPC231S-Q1 to
specify the brightness level of the system. At start-up, the calibration
data provides a default dimming level.
- Based on the dimming level
and calibration data, the DLPC231S-Q1 Software
determines the correct LED sequence and TPS99000S-Q1 register settings. The LED sequence is the order and
timing of LED pulses. TPS99000S-Q1 register
settings determine the brightness of the LED pulses.
- The LED sequence determined
by calibration data is requested to be loaded from external flash to the
sequencer memory. The sequencer block uses the sequence loaded into its
memory to send LED select signals to the TPS99000S-Q1. These signals control the enable and disable for
individual LEDs.
- LED brightness is regulated
to the level requested by the DLPC231S-Q1 via a
feedback loop consisting of the TPS99000S-Q1,
LM3409, the LEDs, and a photo-diode. The brightness target is set by the DLPC231S-Q1 into a DAC in the TPS99000S-Q1. LED brightness is measured by a photo-diode and
trans-impedance amplifier (TIA) inside the TPS99000S-Q1. The target brightness and the measured brightness
are compared by a comparator in the TPS99000S-Q1.
The output of the comparator is used for hysteretic control of the LED light
level.
Figure 6-9 shows an overview of all of the monitoring and diagnostics BISTs included in the
DLP4620S-Q1 chipset.