SFFS764 July 2024 REF35-Q1
This section provides a failure mode analysis (FMA) for the pins of the REF35-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality. |
B | No device damage, but loss of functionality. |
C | No device damage, but performance degradation. |
D | No device damage, no impact to functionality or performance. |
Figure 4-1 shows the REF35-Q1 pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the REF35-Q1 data sheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
GND | 1 | Normal Operation. | D |
GND | 2 | Normal Operation. | D |
EN | 3 | The device is in shutdown mode. | B |
VIN | 4 | The device has no power for normal operation | B |
NR | 5 | No damage to device. The output does not regulate and is held low. | B |
VREF | 6 | Potential device damage due to short circuit current. Not recommended condition. | A |
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
GND | 1 | No damage to device. The output does not regulate and is held low. | B |
GND | 2 | No damage to device. The output does not regulate and is held low. | B |
EN | 3 | Normal operation. This pin can be left floating. | D |
VIN | 4 | Device is unpowered. | B |
NR | 5 | No damage to device. No impact to functionality. | D |
VREF | 6 | No damage to device. No impact to functionality. | D |
Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|---|
GND | 1 | GND | Normal Operation. | D |
GND | 2 | EN | Loss of enable and disable functionslity. The device is in shutdown mode. | B |
EN | 3 | VIN | Loss of enable and disable functionality. The device is in active mode. | B |
VIN | 4 | NR | No damage to device. The output does not regulate and follows Vin | B |
NR | 5 | VREF | No damage to device. NR pin pull more current than expected. Performance degration. | C |
VREF | 6 | GND | Potential device damage while powering up. Not recommended condition. | A |
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
GND | 1 | The device has no power for normal operation | B |
GND | 2 | The device has no power for normal operation | B |
EN | 3 | Loss of enable and disable functionality. | B |
VIN | 4 | Normal operation. | D |
NR | 5 | No damage to device. The output does not regulate and follows Vin | B |
VREF | 6 | Large current can flow into VREF , which can cause permanent damage | A |