SFFS779 December 2024 TMS320F28P550SJ
This section provides a brief summary of the diagnostic mechanisms available on the TMS320F28P55x MCU device family. The diagnostic mechanisms are arranged as per the device portioning given in Figure 5-1. At places where the safety mechanism is applicable for more than one component, the safety mechanism is placed at an appropriate place based on the applicable use-case scenario. For a detailed description or implementation details for a diagnostic, refer to the device-specific technical reference manual.