SFFS779 December 2024 TMS320F28P550SJ
This section contains a brief description of the elements on the TMS320F28P55x MCU device family, organized based on the classification of generic hardware parts of a system [8], as indicated in Figure 5-1. For a full functional description of any of these modules, refer to the device-specific technical reference manual. The brief description of the hardware part is followed by the list of primary safety mechanisms that can be employed to provide diagnostic coverage to the hardware part. Some safety standards have the requirement to provide diagnostic coverage for the primary diagnostic measures (for example, latent fault metric requirement from ISO26262). These measures are called as test for diagnostics. Primary diagnostics, of type Software and Hardware|Software, involve execution of the software on the processing units using the CPU and CLA and also using many of the MCU parts, like Interconnect, memory (Flash, SRAM, and ROM), and TMS320F28P55x MCU infrastructure components (Clock, Power, Reset, and JTAG). To maintain integrity of the implemented primary diagnostics and the associated diagnostic coverage values, measures to protect the execution of primary diagnostics on respective processing units must be implemented. TI recommends an appropriate combination of tests for diagnostics is implemented for parts of the MCU that contribute to the successful operation of the processing units. For diagnostics of these parts, refer to the respective sections in this safety manual. In cases where separate tests for diagnostic measures exist for a primary diagnostic measure, those tests are mentioned along with the respective hardware part.