SFFS779 December 2024 TMS320F28P550SJ
Embedded pattern generator (EPG) can be used to check the functionality of several communications on the device by driving a known pattern on the receive input pin and comparing the received message. EPG loopback can also be used to inject errors on the receive line and to check the diagnostics of the peripherals, such as the CAN CRC logic operation, which is indicated by an error interrupt. Refer to the device-specific technical reference manual for more information about EPG.