SFFS818 March   2024 SN74AXC2T45-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a Failure Mode Analysis (FMA) for the pins of the SN74AXC2T45-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 4-2 through Table 4-6 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality
BNo device damage, but loss of functionality
CNo device damage, but performance degradation
DNo device damage, no impact to functionality or performance

Figure 4-1 shows the SN74AXC2T45-Q1 pin diagram. For a detailed description of the device pins please refer to the 'Pin Configuration and Functions' section in the SN74AXC2T45-Q1 data sheet.

GUID-69069C24-A224-4039-846C-7F611D89CFE6-low.gif Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA1GND short to VCC, device will be bypassed; may cause system damage, but damage to the device does not occurB
A12If configured as an output then damage is possible. If configured as input, no damage, but output will not switchA
A23If configured as an output then damage is possible. If configured as input, no damage, but output will not switchA
GND4Normal OperationD
DIR5Direction control will fix B --> A directionB
B26If configured as an output then damage is possible. If configured as input, no damage, but output will not switchA
B17If configured as an output then damage is possible. If configured as input, no damage occurs, but output will not switchA
VCCB8GND short to VCC, device will be bypassed; may cause system damage, but damage to the device does not occurB
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA1Device will not be poweredB
A12If configured as output, normal operation. If configured as input, no damage, but output will not switchB
A23If configured as output, normal operation. If configured as input, no damage, but output will not switchB
GND4Device will not be poweredB
DIR5Direction control will fix B --> A directionB
B26If configured as output, normal operation. If configured as input, no damage, but output will not switchB
B17If configured as output, normal operation. If configured as input, no damage, but output will not switchB
VCCB8Device will not be poweredB
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effect(s) Failure Effect Class
VCCA 1 A1 If configured as an output then damage is possible. If configured as input, no damage occurs, but output will not switch A
A1 2 A2 Two inputs shorted together will not cause damage unless there is external bus contention that drives the input such that VIL < Input Voltage < VIH in which case excessive supply current to GND may cause damage. Two outputs shorted together may cause damage if there is external bus contention that drives one output LOW while driving the other output HIGH. If both outputs are HIGH or both outputs are LOW, then nothing will occur; no damage. A
A2 3 GND If configured as an output then damage is possible. If configured as input, no damage, but output will not switch A
GND 4 DIR Direction control will fix B --> A direction B
DIR 5 B2 If DIR is LOW, B will be an input and drive the output low. If DIR is HIGH, B will be an output and damage is possible based on state of A A
B2 6 B1 Two inputs shorted together will not cause damage unless there is external bus contention that drives the input such that VIL is less than Input Voltage is less than VIH in which case excessive supply current to GND may cause damage. Two outputs shorted together may cause damage if there is external bus contention that drives one output LOW while driving the other output HIGH. If both outputs are HIGH or both outputs are LOW, then nothing will occur, no damage occurs. A
B1 7 VCCB If configured as an output then damage is possible. If configured as input, no damage occurs, but output will not switch A
VCCB 8 VCCA VCCB short to VCCA, device will be bypassed; may cause system damage, but no damage to the device occurs B
Table 4-5 Pin FMA for Device Pins Short-Circuited to VCCA
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
VCCA 1 Normal Operation D
A1 2 If configured as an output then damage is possible. If configured as input, no damage occurs, but output will not switch A
A2 3 If configured as an output then damage is possible. If configured as input, no damage occurs, but output will not switch A
GND 4 GND short to VCC, device will be bypassed; may cause system damage, but no damage to the device occurs B
DIR 5 Direction control will fix A --> B direction B
B2 6 If configured as an output then damage is possible. If configured as input, damage is possible if VIH/VIL is not met A
B1 7 If configured as an output then damage is possible. If configured as input, damage is possible if VIH/VIL is not met A
VCCB 8 VCCA short to VCCB, device will be bypassed; may cause system damage, but no damage to the device occurs B
Table 4-6 Pin FMA for Device Pins Short-Circuited to VCCB
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
VCCA 1 VCCB short to VCCA, device will be bypassed - may cause system damage, but damage to the device does not occur B
A1 2 If configured as an output then damage is possible. If configured as input, damage is possible if VIH/VIL is not met A
A2 3 If configured as an output then damage is possible. If configured as input, damage is possible if VIH/VIL is not met A
GND 4 GND short to VCC, device will be bypassed; may cause system damage, but damage to the device does not occur B
DIR 5 If VCCB>VCCA, DIR will fix B --> A direction OR if VCCB<VCCA, input could be inappropriate logic level potentially causing damage A
B2 6 If configured as an output then damage is possible. If configured as input, damage does not occur, but output will not switch A
B1 7 If configured as an output then damage is possible. If configured as input, damage does not occur, but output will not switch A
VCCB 8 Normal Operation D