SFFS868 April   2024 ISOM8110-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
    1. 2.1 ISOM811(0-3)-Q1 DFG Package
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
    1. 4.1 ISOM811(0-3)-Q1

ISOM811(0-3)-Q1

This section provides a failure mode analysis (FMA) for the pins of the ISOM811(0-3)-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to supply (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality.
BNo device damage, but loss of functionality.
CNo device damage, but performance degradation.
DNo device damage, no impact to functionality or performance.

Figure 4-1 shows the ISOM811(0-3)-Q1 pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the ISOM811x-Q1 data sheet.

GUID-20230506-SS0I-TSPC-MMSJ-LF9DSK98DKDB-low.svg Figure 4-1 ISOM811(0-3)-Q1 Pin Diagram
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
AN 1 No power to the device so output is in default state. B
CAT 2 Normal functionality D
EM 3 Normal functionality D
COL 4 Output state is undetermined. B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
AN 1 No power to the device so output is in default state B
CAT 2 No power to the device so output is in default state B
EM 3 Output state is undetermined. B
COL 4 Output state is undetermined. B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effects Failure Effect Class
AN 1 CAT No power to the device so output is in default state. B
CAT 2 AN No power to the device so output is in default state. B
EM 3 COL Output state is undetermined. B
COL 4 EM Output state is undetermined B
Table 4-5 Pin FMA for Device Pins Short-Circuited to supply
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
AN 1 If the supply voltage is greater than VF, the device gets damaged with not current limiting resistor A
CAT 2 No power to the device so output is in default state. B
EM 3 Output state is undetermined. B
COL 4 Output state is undetermined. B