SFFS889 July 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
Integrity of the ADC can be checked by monitoring the DAC output using the ADC. DAC in the CMPSS can be configured through software to provide a set of predetermined voltage levels. These voltage levels can be measured by the ADC and the results obtained can be cross-checked against the expected values to verify proper functioning of the ADC. This technique can be applied during run time to verify that proper voltage levels are driven from CMPSS DAC.
For more information on the CMPSS DAC channels that can be sampled by the ADC without external, board-level connections, see the device-specific data sheet or technical reference manual. Additionally, the input signal to the ADC must not be driven by any other sources while the test is performed.