SFFS889 July 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
The ADC SOC (start of conversion) signal input to the ADC module can be triggered by multiple sources, including software, CPU Timers, GPIO, ePWM module instances, and so forth. A fault originating from a peripheral not used in implementing the safety function and cascading into the ADC can cause interference. To achieve freedom from interference, TI recommends that the application only enables the required SOC triggers. This practice avoids faults that originate from an outside source impacting the functionality of the ADC.