SFFS889 July 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
The flash modules implemented in the TMS320F280013x MCU device family have a bit multiplexing scheme implemented, so that the bits accessed to generate a logical (CPU) word are not physically adjacent. This scheme helps to reduce the probability of physical multi-bit faults resulting in logical multi-bit faults. Rather, the faults manifest as multiple single-bit faults. Since the SECDED flash ECC can correct a single-bit fault and can detect a double-bit fault in a logical word, this scheme improves the usefulness of the flash ECC diagnostic. Bit multiplexing is a feature of the flash memory and cannot be modified by the software.