SFFS889 July 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
To stay as general as possible, the functional safety concept assumes the MCU is playing the role of a processing unit (or part of the unit) and connecting to remote controllers by means of a communication bus, as shown in Figure 4-2. The communication bus is directly, or indirectly, connected to sensors and actuators.
IEC 61508-1:2010 defines a compliant item as any item (for example an element) on which a claim is being made with respect to the clauses of IEC 61508:2010 series. A system including the TMS320F280013x microcontroller, as indicated by Figure 4-2, can be used in a compliant item according to IEC 61508:2010.