SFFS889 July 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
The HRPWM module extends the time resolution capabilities of the conventionally derived digital pulse width modulator (PWM). HRPWM is typically used when PWM resolution falls below approximately 9-10 bits. The HRPWM is based on micro edge positioner (MEP) technology. MEP logic is capable of positioning an edge very finely by subdividing one coarse system clock of a conventional PWM generator. The time step accuracy is of the order of 150ps.
The following tests can be applied as diagnostics for this module (to provide diagnostic coverage on a specific function):