SFFS889 July 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
External signal sources vary in their ability to drive an analog signal quickly and effectively. To achieve rated resolution, the signal source must charge the sampling capacitor in the ADC core to within 0.5 LSBs of the signal voltage. The acquisition window is the amount of time the sampling capacitor is allowed to charge and is configurable for SOCx by the ADCSOCxCTL.ACQPS register. This configurable parameter can be used to provide diagnostic coverage for the input signal path and ADC sampling capacitor logic. The test can be done by redundant conversion of the same input signal by the ADC using the preset ACQPS configuration and an ACQPS configuration set higher than the preset configuration. The results obtained must be within a pre-defined range determined by the application and the ADC specification parameters.