SFFS889 July 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
The link pointer OTP location is not protected by ECC. To provide better security to the customer code and enable application safety, majority voting and data consistency-based error detection are implemented. The location of the zone select region in OTP is decided based on the value of three 29-bit link pointers (Zx-LINKPOINTERx) programmed in the OTP of each zone. The final value of the link pointer is resolved in hardware when a dummy read is issued to all the link pointers by comparing all three values (bit-wise voting logic). Any error in the resolution of the final link pointer value sets the Zx_LINKPOINTERERR register.