SFFS889 July 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
Due to the inherent versatility of the device architecture, several software voting-based functional safety configurations are possible. While implementing these configurations, the system integrator must consider the potential common-mode failures and address these failures in an appropriate manner. These failures can be addressed by adapting TMS320F280013x requirements based on the availability of processing units. As stated earlier, the device claims no hardware fault tolerance, (for example, no claims of HFT > 0), as defined in IEC 61508:2010.
The major safety features of TMS320F280013x are shown in Figure 4-3.