SFFS889 July 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
ePWM is typically used as the output signal in closed-loop control applications such as EV traction, DC-DC, and industrial drive. In such applications, failures in the ePWM output, such as stuck-at fault or frequency or duty cycle change, results in disturbance to control loop parameters or variables, leading to conditions such as overvoltage, overcurrent, or overtemperature. By monitoring characteristics of these control loop parameters implemented at the application-level, faults in the ePWM module can be detected.