SFFS889 July 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
On receiving an NMI, the software can attempt recovery from the NMI condition. Based on the severity and type of the fault condition, recovery can not always be successful. In such a situation, an additional protection is provided by having an independent watchdog monitoring the NMI recovery. If the attempted recovery is not successful, a reset is issued. The timeout for reset can be configured (using NMIWDPRD) based on the FTTI of the device.